I have recently attempted to use the TPS53355 for a simple high-current buck converter. I used the WEBENCH Design Tool to get an automated design from TI for the following specs:
- Vin: 6-15V
- Vout: 5V
- Iout: 30A
I then looked over the schematic and ordered all the required external parts. I created the circuit but it gave quite odd results. To test it, I used an input of 9.12V from a 9V battery. The output resulted in roughly 2-2.25V rather than the expected 5V. I tried an input of 12.91V from another supply and the circuit output was roughly 3.6-3.7V. I then realized that through creating the circuit, I had forgotten to put the TPS53355's PWPD to Ground. So I put it to ground and the new voltage was 0V, regardless of input voltage. I rebuilt the circuit 4 times to ensure I didn't do something wrong but the same results occured each time. At this point, I assumed at some point I may have killed the TPS53355 so I ordered a new one. It can today and when I tried to use it, the same results as previously mentioned occured (albeit, at about 0.2V higher).
If someone has any reasonable explanation for what I may have done wrong, please let me know. I'm especially confused by the fact there is only an output voltage without PWPD connected to ground.
Thanks.
(The schematic that TI generated for the given specs is shown below)