Dear TI-er.
My customer was tested TLV62090EVM-125.
Test condition : Output Load is 2.5V & 1.2A.
My customer's Question
1) SW(Pin 1& 2)'s frequency is changed by input voltage. What is that ?
2) The Frequency isn't trigerring. What is that ?
Input voltage is 3.4V. and It is triggered.
Input voltage is 3.1V.
Input voltage is 3.2V.
Input voltage is 3.3V.
Input voltage is 3.4V.