Tool/software: WEBENCH® Design Tools
Hello,
We used TPS54232 for a buck project based on Webench design, which on previous projects, webench was pretty accurate and now there is an issue with insufficient current when testing the circuit with load.
The circuit outputs 5.17v which is ok but the MAX current is 250 to 300mA in 4v and less... if increasing the load, it drops even to 2v without increasing the current (Vin in this case was 13v).
Question is, why its happened? what components/ values need to be replace in this design?
I made a new webench design with the same requirements and it gave three different parameters from the last time (RCOMP=49.9K, COMP2=10PF, COUT=22UF) I changed this three instead of the basic design and it did not influenced the current...
VIN 10.5V - 27V
VOUT 5.15V
I OUT 1.5A
Attached the schematic and the new webench design for reference.
Appreciate your Assistance!
Thank you,