This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62746: Output Voltage Setting

Part Number: TPS62746
Other Parts Discussed in Thread: TPS62743, TPS62745

I am considering the use of TPS62746 in a current design. In its datasheet Figure 8 shows an efficiency plot for VOUT=3.3V. However Table 1 seems to imply that only 1V2 and 1V8 outputs are available. Which is correct?

The parametric search also implies that the TPS62746 has a max output voltage of 3.1V.