HI,
I am using TPS65261-1 and it is mention in datasheet that 10uF capacitor at input side for each pin PVIN1,PVIN2,PVIN3,VIN.Does it mean to connect four 10UF decap at each input pin?Or if i am connecting all four pin together then one 10UF capacitor is enough for operation?
I am using 12V as input supply.
One more doubt i have regarding the VDIV pin of TPS65261-1 device.What should be the voltage level for this pin?I am connecting this this pin to 12V supply so what should be the resistor divider need to be required to use?
Thanks
Ashutosh