TPS54040A Enable threshold voltage is Min:1.11V Typ:1.25V Max:1.36V (@TJ = –40°C to 150°C, VIN = 3.5 to 42V)
Please let us know Enable threshold voltage (@–25°C to 85°C)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.