Hello,
I am working on reliability of converter circuit for a motor application. We have used MC33063A-Q1 as a buck converter. It is used for 12 V to 5V/200 mA conversion on that converter board. The IC gets short at around 65-degree centigrade ambient temperature. As per the datasheet, working temperature is -40 to 125-degree centigrade.
Before thisI had used MC34063ADE4, its operating range is 0-70 degree centigrade. The same mentioned IC used to get short at around 80-degree centigrade ambient temperature. As per the datasheet, it looks fine. The current IC MC33063A-Q1 is meant for higher temperature, but it is actually getting short at around 65-degree centigrade.
As the temperature falls below 40-degree centigrade it starts operating normally. Could you please let me know the reason behind this issue.
Thank you