Hi,
We got a question from customer about LMR14030-Q1.
Could you help us?
[Question]
When the IC turns on at Vin=16V and no load, the ringing occur on SW. Please refer to below screenshot.
They are concerned that this phenomenon is abnormal of the IC. Why does this ringing occur?
- Condition -
Vin=16V
Vout=5V
Iout=0A
fsw=2.1MHz
*When Vin=12V, there is no ringing on SW.
Best Regards,
tateo