Please suggest Boost converter IC For following specification.
Vin- 5 V to 18 V
Vout- 24 V 2-3A
** Form factor of IC is not concerned.
**Required Minimal component.
**Should Not be complex design.
**Non Isolated DC/DC
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The integrated boost controller is not fit for this application as the output power is really high.
Suggest you use Boost controller LM3478/81. The circuit is simple. you can found the related schematic from the datasheet.
You can open a new post if you interested in it. The rellated person will help you.