Other Parts Discussed in Thread: TPS54200, INA199
Hello all,
I've being using the TPS54200EVM to develop a battery charger for a health application. In order to test it, I tried using the Battery emulator mentioned in the following link. The charging profile is assured by a MSP430 that will generate the TPS54200`s PWM input signal, according to the Battery emulator's charge.
The problem is when I assembled all of the system, the supply voltages dropped (in what seemed to be a great current increase). I checked the TPS54200 if I still had any current flowing out but I couldn't measure anything. The feedback voltage also gave me nothing.
I took the TPS54200EVM out of the circuitry and did some measuring a part. With a 12V Vin and a 3.3V 50KHz PWM signal I had absolutely nothing at the output. I tried using various power resistors (3.3 Ohm, 5Ohm, 13Ohm). I still had nothing on the output. I wonder if there is something wrong with the IC. Measuring direcly at the IC"s pads I verified that the integrated regulator is still delivering 6V as described in the datasheet for Vin> 6V. No signal is being delivered out the SW pad.
I ordered some TPS54200 samples so I can change it at the EVM if needed. But before doing such a thing, do you think there is any other test I can make to verify that the IC is actually fried?
I used a LRC meter and a voltmeter to verify that the passive components are still functioning , and it appears that C4 is no longer good. Could he be the reason the EVM is not functioning properly?
I thank you in advance for the help.
Patrick