Hi Team,
Do we have a device in our portfolio that is a true negative supply? Something to displace the LTC7149..
Thank you,
Jared
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi John,
I am looking for something that is properly ground referenced.
i.e. the LTC7149's ground pin is actually connected to ground:
I have looked at this link for solutions from our portfolio, but for all our solutions the ground is referenced to the negative supply:
Here is why a true negative supply is desired: When a positive switching power supply is connected in the negative configuration, it is possible to have currents that back flow from the output of the supply to the digital interface controlling the power supply. True negative supplies have an interface designed to be connected up to controlling logic with no inversion.
Here are the requirements trying to be met:
Input: 24V
Output: -20V
Output Current: ~250mA
Power good feature.
Looking forward to your feedback
-Jared
So it does not sounds like we have a inverting power supply where the ground pin is ground referenced, correct?
Those were the parts my search revealed. As a disclaimer, my group would not have anything to offer, but maybe someone else knows of something.
Hello Jared,
If you are searching for a part from 24V input voltage, I do not know of any in the portfolio I know, but we have several that are going from +5V to -5V, e.g. TPS63700 or TPS60400. And some that have 2 outputs, one positive and one negative one, e.g. TPS65130
What is the reason that you want to have the GND pin referenced to the system GND?
Best regards,
Brigitte
Hi Brigitte,
Thank you very much for the suggestions! The reason I want to have the GND pin referenced to the system GND is based upon what I mentioned above..
Here is why a true negative supply is desired: When a positive switching power supply is connected in the negative configuration, it is possible to have currents that back flow from the output of the supply to the digital interface controlling the power supply. True negative supplies have an interface designed to be connected up to controlling logic with no inversion.
Thank you!
Jared