Other Parts Discussed in Thread: LM3488
Hi, team.
In selecting this IC, I would like to investigate the fluctuation rate of the feedback voltage under the following conditions, is it possible?
Condition: Switching frequency 100kHz
Vin = 24V (± 10% or ± 5%)
Operating ambient temperature -10℃~60℃
As for data, I would like if there is temperature characteristic and Vin characteristic of VFB.
Could you help us?
Best regards,
Masumi Sekiguchi