Other Parts Discussed in Thread: LM5122
I have a boost power supply application that is somewhat beyond the limits that is supported on Webench. I chose a design that is about as close as I could find and planned to modify it.
Here are my requirements: Input: 10-36V, Output: 48V, Current: 13 amps, nominal with up to 30 peak amps
The power supply will be used to power a DC motor in a large power tool. I have added 10 MOVs to the output circuit, mainly to protect the output diode, as well as the other circuits.
Webench provided a 10 amp suggested design. I made a PCB for the circuit and it boosts the voltage to 48V with no load. It seems to work Ok at about 3 amps. But if put a 10A load on it, the chip and the MOSFET fail and have to be replaced. I would think the cycle-by-cycle current limiting feature would protect the MSFET and the chip from overcurrent damage, if the design is correct. The circuit also seems a bit unstable at higher currents, meaning the output current goes up and down before the circuit fails.
I have a few basic questions, to begin with:
1. I would like to know if there is any reason I cannot use the LM5022 chip for the 13 amp/30 peak amp application. The datasheet does not say there is a current limit, and the chip doesn't contain any power FETs or handle the high current directly.
2. I am puzzled by the failure of the LM5022 chip. I have replaced a couple of them and it's a mystery to me why they're failing. Any insights will be very helpful.
3. I am entering the dozens of formulas that are provided in the datasheet to calculate the values for each part, and checking the spreadsheet calculations by the examples in the datasheet. I will then use the spreadsheet to calculate the values for the higher current. Do you think there will be a problem with that? I'm assuming I need to use 30 amps as the output current, even though that is the peak amps.
4. Do you have any other advice or suggestions you think I should know about?
This is a proof of concept prototype for potentially high volume application, and worthy of some good technical support. I'm on a short time frame and I need to get this circuit working next week. I'm not a power engineer, and my experience is with lower power boost regulator applications. Any help you can provide will be invaluable. If there is a better chip to use in the production design, that's no problem at all. But I have a lot invested in the LM5022 and not much time to change direction, if the LM5022 chip can do the job.
Thanks very much.
Charlie Weisel