Other Parts Discussed in Thread: LP5907, TPS61029, TPS61020, TPS61252, ESD401
Hi all!
We tested our device in an ESD testing laboratory, and we fail on -8kV voltage (the +8kV was OK).
After i take apart the whole device , and looking for errors, i found out that the problem is with the TPS61028 , which is providing us an 5,4V for our 5V power supply LDO-s.
As i measure, the TPS61028 EN pin has a closure with the GND (measure about 5 Ohm-s).
The TPS power input is on a power bus (getting power from a galvanic isolated DC/DC, 4.7-4.8V), with this voltage we feed a few LDO-s which does need a voltage above 5V to give us the other working voltages (3.3V,2.5V..etc). The strange situation is that there is no problem with any of the element which are located on this A+5V bus (what can seen on part of the schematic), but the problem is only with this part.
The enclosure is from metal, but we have a plastic cover.
The metal enclosure does not connects to the section where is the TPS61028 located. The metal shield is connected to the part (through a 6.3kV, 1000pF capacitor) on which is the galvanic isolated dc/dc input part.
Between the DC/DC input output island is also a 6.3kV capacitor (2.2nF).
So the matal enclosure is not connected electrically to the TPS61028.
we checked the whole board, and the problem is only with the TPS61028, and only with its EN leg...
If i power on only the TPS, it is working(but it eats about 300mA by itself...., previously the whole board consume this amount of current)
Currently we are thinking where the -8kV comes in, and how is it possible that no one of the other elements(LP5907, TPS73125, etc) located on the same A+5V bus are fine, and without any problem.
Did someone has same situation , or similar with this TPS61028?
Thanks in advice!
Best Regards
Lou