This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65131: Negative Channel Produces No Output

Part Number: TPS65131

I am using the TPS65131 split rail converter to generate +12V and -12V from +5V input. Schematic is shown below and is very similar to that shown in the datasheet. +12V output works fine, but the -12V side reads -0.21V.  VREF checks out at 1.22 V.  FBP measures 1.47V, FBN measures 1.08V.  Voltage at OUTN is a couple millivolts.  I do have the PSN terminal tied high and was wondering if that is what is disabling the negative output.   Is there a minimum current required to enable the output?  The board layout looks good and I have checked all traces. Is there anything in the board layout that would cause the negative side to act like it is turned off

 

  • Hello James,

    The schematic looks as expected, although I did not go through the external component calculations.

    The converter seems not to switch at all. Please check out the startup behavior with a scope because I expect that it tries to start and then does stop because of a problem. Dependent on the problem, the IC could be damaged already as well.

    Layout could cause such a problem even if it looks ok. We would need to have a more detailed look on it, especially if the switch node is causing some problems on the CN or FBN pins.
    If layout is the last option that is left, I think it is best that you check out the EVM of this device and try to get very close to this one.

    Best regards,
    Brigitte
  • Hello James,

    Do you have any feedback for us? Could you send us the layout and some scope plots to show the behavior?

    Thank you.
    Best Regards.
    Ilona