Other Parts Discussed in Thread: LMR16006
Hi!
I am working with LMR16006Y first time, and I need help in assessing the correctness of the layout of the circuit. All parts were calculated according datasheet with output current less than 100mA.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi!
I am working with LMR16006Y first time, and I need help in assessing the correctness of the layout of the circuit. All parts were calculated according datasheet with output current less than 100mA.
I think your schematic and layout are fair.
I have the following comments:
1. I would increase the value of C12/16 to 10uF
2. Need many more ground vias around C12/16, D4/5, C14/18 and the ground of the device. This will help to connect the grounds better.
3. Connect top of R3/6 closer to C12/16
4. Use as wide a trace as possible to pin2 ground.