Other Parts Discussed in Thread: LM5088, , LM5085
Hi TI,
we are using the LM5010 in an application with 30V - 50V input and 24V output voltage. We have a wide range of output current from 1mA to 1A. The output voltage gets too low with low output current and low input voltage. Is this type of regulator not optimal for this range of output current? Would LM5088 be a better choice?
It could be helpful if the webbench also had an option for output current range that could guide us to the best controller with respect to this demand.
regards Trond Inge Wang