In optimizing the design at hand (externally synchronized boost converter) I ran into the puzzeling statement from the datasheet (page 9, paragraph 7.3.3) which states "The sync pulse width
measured at the RT pin must have a duration greater than 15 ns and less than 5% of the switching period".
In my case (frequency = 502kHz) this pulse would therefore need to be between 15 and 99 ns.
Based on the other information given in that same paragraph, I conclude that the time constant of the differentiating network formed by the timing resistor RT and the coupling capacitor must be roughly the same value.
Given the required RT of 24.9kΩ the time constant of the differentiating network, formed with the recommended 100pF coupling capacitor is 2.5ns 2.5us; which would mean this pulse will be way too short long...
What am I missing here?