Hi all
Would you mind if we ask LM5166?
<Question1>
In case of LM5166Y(3.3V fixed), the datasheet shows REGULATION COMPARATOR is Min=3.23V and Max=3.37V.
Does it mean that output voltage accuracy is Min=3.23V and Max=3.37V?
So, does it contain COT and PFM mode?
<Question2>
Our customer uses LM5166(adj type).
And then, output voltage is 3.1V, Iout=75mA.
According to changing input voltage, output voltage changes.
-Input 12V : 3.190V
-Input 8V : 3.170V
-Input 14V : 3.220V
Our customer doesn't have wave form, however Ton depends on Vin, so Vout changes.
Is our recognition correct?
Kind regards,
Hirotaka Matsumoto