This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

LM5166: Quiescent current in dropout

Part Number: LM5166

I have a design which accepts an input in the range 10V - 24V, and must limit the output to 12V nominal, over a range of loads from 0 to 300mA.This is a low power application so quiescent current is important. I can tell from the datasheet what the device quiescent current will be in regulation, but I can't tell what current draw will be in dropout, at 100% duty cycle, in PFM mode.

  • Hello Richard,

    With the FB pin being low in Drop out mode, the part will be active. Please refer to the datasheet for active IQ specification in PFM.

  • In reply to David Baba:

    Thanks David. I was afraid that was going to be the answer.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.