Other Parts Discussed in Thread: LM3478, LM5121, LM3481
tps43061 very advantageous feature is 5.5v mosfet gate drive. this reduces power losses vs 7.5v drive. that alone dictates using tps43061.
my dc-dc is 19.5v in, 34v out, 4.2A out. I want top efficiency, 98.5% using webench. my lm3478 webench is 98.5%, using all custom components, but tps43061 has few components, and no custom mosfet at all.
I reported this limitation separately yesterday. can't webench tps43061 with good parts, only 4 poor performing parts that TI supplied.
FLASH!! this afternoon, there are now 40 items, most are quadraplets (4X, same part). still not good, many mosfets are duals. dual mosfets have poor rdson and Qc.
question: it is nice to have uvlo (which happens if output is shorted), then the boost circuit shuts down. circuit is protected from output shorts? is this correct?
question: I found a schottky diode with much lower power loss (1/2) than using best mosfet. thus there is not efficiency gain using a mosfet. it is ok to not connect HDRV?
note: read and searched 100 pdfs regarding mosfet vs. diode, about 2/3 of them end up with a schottky diode (smaller) anyway, to reduce the mosfet diode losses. every single pdf uses a relatively high voltage drop diode for analysis. I searched thoroughly in TI, ONsemi, vishay, and 5 others for a mosfet that has lower loss than the diode. none. so is synchronous rectification all blown out of proportion? hype?
question2: if I use a 2nd mosfet as shown in tps43061 schematic, then if my output has a short, will the 2nd mosfet burn out since it is directly connected to input? many pdfs said the mosfet conducts both ways. the tps43061 pdf does not mention what happens if output is shorted. if I need to protect the mosfet from damage, and the mosfet is there to "prevent" damage, then I'm not using a 2nd mosfet for rectification.