Hello TI,
1. Does TI WEBENCH also account for the AC losses when calculating the inductor power dissipation?
2. Selecting an inductor with lowest DC resistance will give the best efficiency. What other parameters of the inductor should be taken into consideration when considering the light load efficiency? We want the switching convertor to consume as little current as possible under light loads.
3. I'm trying to find a suitable inductor for our design with the LMR23630A (400 kHz) which will power a GSM modem. WEBENCH suggests the Coiltronics XAL7030-822. An application note from Würth Elektronik mentions that for switching frequencies between 100kHz and 1000 kHz it is better to use ferrite and to use iron powder for less than 100 kHz. How true is this recommendation? Is it still advisable to go ahead with iron powder or other composite cores for the 400 kHz LMR23630A? What disadvantages other than cost would you mention with regard to inductors that have cores other than ferrite?
4. The LMR23630A should also turn on if the EN pin is supplied with a 1.8V, right? The datasheet mentions a threshold of 1.6V.
5. Can the ground pour on the top plane extend all over the PCB? The second layer is a complete ground plane. The datasheet mentions a 'localized' ground plane on the top, can you elaborate on this?