I need an unusual boost converter for a proof-of-concept design.
The input will be a 4S LiPo battery pack, 12-17VDC.
The output is dual rail, +/-65V at 200mA.
The LM5000 looks like it will work for the positive side, but the output voltage is pretty close to 75V max. Is this too close to the max to be reliable?
Also, are there any demo boards that could be modified to evaluate this design?
Any ideas for the negative side (-65V)?