Hi,
I am new in PCB designing I have created a PCB that can boost Lithium Polymer/Ion battery voltages to 5 Volts to drive RGB LEDs (APA102 5050, APA102 3535, APA102 2020, SK6805-2427, SK6812 MINI 3537) from ESP8266 WROOM-02.
I have used this IC after MCP73871, it is used to charge the battery.
I have used these C1 = 10uF (1206 Ceremic) with 0.1uF (0805 Ceremic), C2 = 2.2uF (0805 Ceremic), C3 = 100uF (1210 Ceremic) , at LBO MUN2114T1 with LED and Resistor of 1k ohms is used to check low battery status.
I am facing few problems that which I switch on my circuit I heart unwanted sound from my power side and when the load is increased it become more prominent.And also LED at LBO blinks with low light and when I increase load intensity of this LED increases intead battery is fully charged.
I can provide you pictures or videos please guide me.
I am really losing my hope from my first PCB.