Dear All,
I'd like to understand how to interpret this specification when it comes to calculating voltage on CM pin at a given load current.
What I have interpreted is that if offset is 25mV, then with 4 mOhm current sense resistor, I may read no voltage on CM pin until minimum load current is 357mA. (25mV / 4mOhm * 17.5). Is this understanding correct?
Also, is this offset bidirectional?
Regards,
Sourabh