Hello.
We use in our device the TPS45020 circuit but are not able to find anywhere on the internet 3D model for this device. Do you have same which can you provide us?
Thanks in advance.
Pavel Riha
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello.
We use in our device the TPS45020 circuit but are not able to find anywhere on the internet 3D model for this device. Do you have same which can you provide us?
Thanks in advance.
Pavel Riha
Pavel,
I exported the step model from Altium It is nothing but a rectangular solid with a cylinder in the upper left corner to indicate pin 1 orientation. It is scaled so 1mm = 1 inch. So you get a box with dimensions 3.599" x 3.599" x 1". Do you want that? Or would you rather have a actual size model that shows the pins? 3D CAD is one of my hobbies. I could buld in in 30 minutes this evening or early tomorrow. Let me know.
John, thank you very much for your fast reply.
Let me admit - I am looking for a model with pins.
Thanks in advance.
Pavel
Dear John,
many thanks for your work. 3D model looks nice and works well.
Sorry for my delayed reaction - I was bussy.
Regards from the Czech Republic..
Pavel