Other Parts Discussed in Thread: LMS3655, LM73605,
Hi there,
Do we have any device (or any roadmap devices) similar to XR76205?
It has to be a converter with synchronous rectification.
Thanks!
Best regards,
Roy Hsu
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Roy,
I check data sheet and below eff data for your reference:
Vin : 12V / Vout = 5V / Iout = 5A
LMR14050 eff=88% LM73605 eff=92%
Vin : 12V / Vout = 3.3V / Iout = 5A
LMR14050 eff=83% LM73605 eff=90%
high perfromance LM73605 has better conversion eff than LMR14050 which is more cost-effective.