This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TPS630250: TPS630250 / Maximum output current

Part Number: TPS630250

Hi,

Please let me ask about maximum output current. I know that the maximum output current depend on input and output voltage, but I'm asking it because the maximum output current of efficiency curve in datasheet is 2A. The actual requirement of the customer is 2.3A output current at 2.5V output from Li-Ion battery (3.0V to 4.2V). I could get result without no error from Webench as attached.

webench_design_964463_1036_258173640.pdf

Best Regards,

Satoshi / Japan Disty

  • HI Santoshi-san,

    I could find measurements in our database for this device for the maximum output current for Vout=2.5V.
    the measurements show that the device can deliver 2.3A for your operating conditions: Vin=3.0V to 4.2V and Vout=2.5V.

    As mentioned in the other post (e2e.ti.com/.../2549698,
    I believe a buck converter would be more suitable for this application, for example the TPS62823 : www.ti.com/.../tps62823.pdf

    _____________________________________________________________________

    You may find interesting additional information in our LPDC App Notes

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.