Other Parts Discussed in Thread: TLV61046, LM2623, PGA460
Hi everyone,
I'm using the LM27313 boost converter in an application with a primary battery of 3.6V / 5000mA. I have some trouble due to a drop off voltage. The voltage drop from 3.6V to 2V. Yellow (Voltage: 1V/D) and blue(Current: 60mA/D)
Is there any way to reduce this drop voltage?
I don't know but I'm not probably using the correct part number and there is another one better. My requirements are the following...
I need to boost voltage from a primary battery of 3.6V to 7.5V with a maximum output current of 50mA, and I need that this IC starts in a soft way, in order to avoid peak currents and drop off voltage.
Is there another better alternative for this application?
Best regards.