Hello,
Have you ever seen the following ack(?) pulse from tps53622?
The details are as follows:
[environment]
Host : Intel Xeon
VR_0 (SVID addr 0) : another vendor's VR
VR_1 (SVID addr 1) : TI TPS53622
[issue]
This issue occurs every power-on sequence.
The pulse appears at the same timing.
At the moment, it seems that the pulse is from tps53622.
The reason is as follows:
- the low-voltge-level is as same as tps53622. (not same as VR_0)
- it does not appear, when tps53622 is disabled. (set svid addr 0xF by Fusion Digital Power Designer)
Is there anything for me to confirm?
Thanks,