Hi,
Could you tell me about TPS61088 operation in "2.5V<Vin<2.7V" condition?
Customer useing input voltage range is 2.7V~5V.
(It is 5 V of USB and battery voltage.)
However, when the output current is large,
The input voltage may be dropped (2.5V<Vin<2.7V) in some cases.
Let the following questions from the above background.
1.Is it a problem to use TPS61088 with "2.5V<Vin<2.7V" condition?
2.In the case of "2.5V<Vin<2.7V" condition, can you compensate the electrical characteristics?
If it can not be guaranteed,Can you tell me the items that can not be guaranteed?
Best Regards,
Yusuke/Japan Disty