Hi Sir,
There is a description in datasheet as below.
"If the UVLO pin is pulled below 1.215 V, the regulator enters a standby mode of operation with the soft-start capacitor discharged and outputs disabled, but with the VCC regulator running."
How is the device consumption current at this moment? Is it defined as " UVLO Pull-up Current Source, UVLO = 0 V , 5.4 µA "