Other Parts Discussed in Thread: LM3478
Hi,
I have the question like below, could you please tell me the reason and how to fix the isse? Thanks.
quote:
-------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
I have used approximately 3mH inductor and achieved voltage upto 270V. But problem is the voltage is gradually decreasing (Voltage drops down to 2V it puts continuous on) and the power Mosfet is heating too much.
As per datasheet Vout= 1.25(1+R2/R1), which indicates it is depending on resistor values. But during testing the output voltage is changing with change in Inductor value. With (10-100) uH inductors voltage is ~100V. When used (1-3) mH Inductors voltage rise to ~ 270V.
Please suggest how should I achieve this much of stable voltage without heating the components.
-------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------