Greetings!
I have searched through the forums. Tried to use the Workbench, but it seems that a problem I have encountered is of another nature.
I have designed a PCB where I use LM2733 as a source for a ~500 mA load.
I use this one instead of the LT1615 device. So it is featable to the same pattern. I use a 2.2u as a IN cap. 4.7u as a OUT cap. 82p in parallel with R1. Feedback is 2.2meg R1 and 91k for R2. The diode is MBR0530. The inductor is LQH3NPN220MM0.
When there is no load and when I start with 12V at the input I get 12V at the output. When I lower the VIN to 1.8V - the VOUT uppers to 30V.
When I put a 590 Ohm resistor in series with the VOUT I get around 22-24 volts at the output and 0.9 volts at the feedback.
Could you please provide me with help! I am truly ashamed also because I thought of ISW as of the output current available.
Thanks in advance
Alexander