Hi everybody,
im using the TPS561201 in a new design, but unfortunately i have an issue i can't solve by myself.
I need the converter to bring 500 mA at 5V. Most of the time it will be at light load, only supplying my MCU.
Testing the circuit i found the TPS over- and undershooting. It also affects the 12V-Supply.
This is the schematic i'm using right behind a Recom Rac AC/DC-module :
This is what the layout looks like:
This are the peaks measured on the 12V supply, which change in frequency:
This is what i measure on 5V at DC/DC output:
Adding a 100µF Elko at 5V output to reduce ripple as test deliveres this:
These measures were all done at almost no load. Putting a restistor the 5V output results in higher frequency of the peaks.
As the inductor the VLS6045EX-4R7M is used.
This problem in reproduceable on an other board with the same layout but without any other parts on it.
I just don't get were the peaks are coming from and really need a solution for this.
Thanks in advance for your help!