This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40211 MR16

Other Parts Discussed in Thread: TPS40211

I gone thru SLVA422, TPS40211 SEPIC MR16 and build a board followed the ref design to drive 4 1W LED in series.

Power source is 12 VAC from 60W Philip E-transformer and covert to DC by rectifier . Facing flickering problem, and draw higher current..

if

Power source is 12VDC. No flickering.