Other Parts Discussed in Thread: LMR33630, TPS62088, TPS62140, TPS82140, TPS62130
Hi,
I've been running some tests with the TPS62822 EVM, and changed the output voltage to 3.3V by changing R1 to 453k. Without load and loads up to 100 mA, the output voltage is a near perfect 3.3V. However, at higher loads (850mA and 1.5A), using resistors as loads, the voltage drops to 3.18V and 3.01V, respectively, even though these currents are well within the device spec. Please advise.
Thanks