Hello,
I have a question about thermal performance for the TPS65251.
We have measured spur performance at the output 1 of the TPS65251 eval. board. Input voltage was 10.2V, output voltage was set to 6.2V. Output current 1.59A (3.9Ohm resistor as a load) and switching freq. 500kHz.
this is measured spurs at the output 1 of the regulator vs temperature (inside the thermal chamber):
spur freq., kHz | power, dBm | |||||
+20C | 0C | -20C | -25C | -30C | -40C * | |
167 | -54 | -54 | -55 | -54 | -54 | -55 |
261 | - | - | -25 | -23 | -21 | -19 |
522 | -27 | -27 | -27 | -27 | -27 | -29 |
784 | - | - | -39 | -39 | -37 | -39 |
*unstable
so only two spurs (167kHz and 522kHz - switching freq.) are presented at the regulator output when the temperature higher than 0C. But for -20C and lower there are two additional spurs appear - 261kHz and 784kHz, and for the temperature -40C output voltage became unstable.
Is it normal behavior for TPS65251?
Is there official information about the operation of the regulator in cold temperature?
Thank you!