Since the current amplifier Vcom(max)=4V. I want to use Current Transformer, not DCR. I have questions:
1. How to make the connection? The block diagram does not show the current amplifier details.
2. What is the maximum Vct(peak) to the input pin?
3. Vct is not of triangle wave. Is it OK?
4. What is the function of the internal differential amplifier internally? I see it is not connected to anywhere. If I want to use it externally, shall I add 4 matched resistors? Why its gain is 1?
5. In my last email, I asked slope compensation. Forget this question because I do not need it due to D < 40%
Please let me know the answer quickly. My design time is tight. Thank you.
Sam