Hi,
I am planning to use TPS65265 as a secondary regulator to generate the following rails:
0.85V @ 5A
1.2V @ 2A
1.8V @ 1A
From reading the datasheet it says that V7V is generated as 6.1V typical, using an LDO from PVIN1=12V. Since an LDO is used clearly V7V must be <4.5V when a 4.5V input voltage is used. Therefore I wanted to confirm that operation from this input voltage will be OK?
In addition it is not explained how the selection of switching frequency should be made. There is a wide range of possible frequencies that could be used. Can a methodology for selection be proposed?
Thanks,
Tom