Other Parts Discussed in Thread: LM5170
Dear Experts,
I would like to develop a bidirectional dc-dc converter using 1 channel from the LM5170-Q1 IC. I have noted these are limited to 60V on the LV side and 85V on the HV side.
I have a bus rail of 48V on the LV battery side and about 200V on the HV side.
What limits the IC to lower voltages? Is it possible to add additional components around the ic to allow high voltages? The power I need to transfer is 1.2kw.
Can use high side drivers to shift HO1 and LO1 and use an opamp to generate CSA 1and 2 signals? is there anything else I can do?
Many thanks in advance
Atish