Hi, I have two questions about the transient response of LM5141.When I change the load current from 0A to 4A,and then change it from 4A to 0A ,why the ripple of output voltage value is different in two different work mode(DEMB mode and FPWM mode)?And why the voltage ripple recover time is longer in DEMB mode than in FPWM mode? The attachment is my test result .Thank you!Transient respond.docx