This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TINA/Spice/LM3478: SEPIC Converter Startup Current Problem

Part Number: LM3478
Other Parts Discussed in Thread: TINA-TI,

Tool/software: TINA-TI or Spice Models

Hi,

I´m designing a power supply (SEPIC Converter) for a circuit wich need an output voltage of 12V. These are the characteristics of the SEPIC:

  • Vin min = 10V
  • Vin max = 30V
  • Vo = 12V
  • Io max = 0,7A
  • Sw Freq = 1MHz

I´ve made a previous design on TINA software and it seems that the supply works fine except for one thing, I obtain a high current at the startup of the simulation. What is the reason of this current? and is it possible to avoid this behaviour?

If someone needs more information I´ll be attentive to provide it. Thank you very much!

Best Regards.

  • Hi Ignacio,

    Can you please show the plot of the output voltage?

    The soft-start of the LM3478 is internal and can be increased by adding the circuit shown below.

    Please let me know if you have any questions.

    Thanks,

    Garrett

  • Yes, sure. Here you have.

    Thanks for your advice. How could I decide Rss and Css values?

    Thank you very much Garrett.

  • Hi Ignacio,

    Please take a look at this application report. This should help explain on how to extend the soft-start time of the LM3478.
    www.ti.com/.../slyt669.pdf

    -Garrett
  • Hi Garrett,

    The increase of soft start doesn´t solve the problem of inrush current at start up. 

    I´ve got 2 real LM3478 samples where I´ve applied my design, the 2 chips have broken-down. I can probe with my multimeter that Isen, Vin, FA/SD and AGND ports are now shorted. 

    I´ve only one more sample and i don´t want to continue making mistakes, so that´s the reason why I´m here.

    Thank you!

  • Hi Ignacio,

    What coupled inductor are you using? 1MHz is a pretty high switching frequency for a SEPIC and the coupled inductor must be selected correctly. Please post the schematic.

    If the pins are shorted it implies that an absolute maximum voltage on one of the pins was exceeded.

    Thanks,

    Garrett
  • Hi Garrett,

    The schematic is the one of my first question. The coupled inductor is 10uH (SRF0703-100M, 0,082Ohm, 2,1A). The mosfet is DMN6140L-7 (I = 2,3A , Vmax = 60V), and the Diode is NTS245SFT1G (Imax = 2A, Vreverse max = 45V).

    I selected this inductor appliying the following formula. I apply a 30% for the ripple current. AIL = 0,7A * (12V/10V) * 30%. L = 10V/(2*AIL*1M)*Dmax (0,55)

    So AIL = 0,25A and L = 11uH.

    Maybe the Isen pin voltage at startup was higher the maximum wich we can see in the datasheet is 500mV. The startup could be the reason of that?

    Thank you Garrett.

  • Any idea Where im failing?

  • Hello again Garret,

    I´ve been investigating on this.

    1. I feel my mistake was connecting the Rsen resistor without a capacitor. Thus, I obtained a peak voltage on the Isen pin higher than 500mV (witch is the maximum voltage allowed). So I decided to connect a capacitor in parallel, and seem it works.

    2. Now, I have a new problem. When the SEPIC is working without load, it works well and it produce 12V.
      But working with load (120Ohm -> 100mA), the Vout goes down to 5 or 6 Volts.
      I neither see a frequency of 1MHz on the DR output.

    Any advice?

    Vout = 12V (Without Load)

    The output without load is 12V, but I obtain some weird noise. This is created together with the DR pin pulse and is transmitted also to the GND.

    ​Vout Fall Down With Load 

    Best regards!