Other Parts Discussed in Thread: , LM5122
I am using EVM TPS43060EVM-199, My Load is switching type ( ON :- 5 ms, OFF :- 5ms, 1.2 Amps MAX)
The Output Voltage dips approx 5 Volts.
Kindly Suggest the solution.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I have checked it with replacing with 100V rated caps.
How to check weather Inductor is not limiting the current or not ?
I will provide the needed plot shortly.
Thanks
Himanshu
Hello Garrett ,
We tried the same test condition with the EVM as well .
24V input 40V output with 15mA to 1.6A transient .
However we saw the issue of undervoltage and overvoltage in the EVM as well , much larger than that shown in the user guide of EVM . we are seeing a dip of 1.2V in our EVM vs 0.7V in the user guide .
Hello,
Is any way to run this device in forced CCM mode? or Is there any other way to reduce the effect of Load transient?
Thanks
Himanshu
Hello,
As per App note
"However, for some low-noise applications or applications requiring a fast transient response from light loads, it may be preferable to sacrifice improved light-load efficiency to keep CCM operation over the entire load range."
What is its meant for user/ designing point of view?
Thanks
Himanshu