Welcome to the Non-Isolated DC/DC Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".
Q: REG710 - The REG710 datasheet shows a different pinout between the QFN and SOT-23 package. Is this correct? by 1166427
Question/Problem:
The REG710 datasheet shows a different pinout between the QFN and SOT-23 package. Is this correct?
Answer:
Yes.
A: Re: REG710 - The REG710 datasheet shows a different pinout between the QFN and SOT-23 package. Is this correct? by 10449
The Jan '09 datasheet is correct. The customer may have either a nonreleased version of the datasheet that was never officially released to the web, or that version of the datasheet was in error and got corrected with a later revision.
Pin 4 is GND
Pin 5 is Enable
Q: Re: REG710 - The REG710 datasheet shows a different pinout between the QFN and SOT-23 package. Is this correct? by 4339
I still need to double confirm the REG71050 TQFN-6 package pin assignment. My customer has different version datasheets on hand, one is from 2008, the other is from 2009. And I also captured in below for reference. You can see pin4 and pin5 are mark reverse. Can you let me know which one is correct?