Welcome to the Non-Isolated DC/DC Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".
Q: TPS62360 Non-I2C by 1294176
Team,
Customer is looking at the TPS62360 for a 1V @ 3A rail, Vin = nominal 3.3V; output voltage regulation of +/- 0.050V. They do not require the output voltage adjustment via I2C. Question -- is Power Save mode the device default, or will the device switch between PWM and Power Save autonomously without an I2C prompt?
A: Re: TPS62360 Non-I2C by 1090425
As noted in the datasheet (table 2), the default operating mode for all VSELx presets in auto PFM/PWM mode. So, the device will enter PFM mode if the load is low enough. They don't need I2C to tell it to.
This part can be operated without the I2C interface. Luckily, the 1V they need is already a pre-programmed preset on the TPS62360.