TPS61020 - Is there an ESD diode between EN and VCC?

Q: TPS61020 - Is there an ESD diode between EN and VCC? by 1166427

Question/Problem:

Is there an ESD diode between EN and VCC?

Answer:

There is no diode between EN and VCC.  The note on page 3 about EN being clamped to VCC or GND only specifies the test conditions.  You can pull EN higher than VCC, however, TI can not guarantee that the current will not rise above the specified and guaranteed limits.  It should not rise above the limits, but this parameter is not tested in production.