Welcome to the Non-Isolated DC/DC Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".
Q: TPS62110 unused open drain-output by 1575317
Hi Team,
Can I ground an unused open drain-outputs on an IC like the TPS62110 and generally other devices like TPS40170. Please advise.
Regards,
Yaser
Q: Re: NU open drain-outputs on TPS62110 and TPS40170 by 10449
A true open drain output can be grounded if not used. If an output's open drain internal FET is on, it just connects the pin to ground. If the FET is not on, it's also ok to connect it to ground.