Q: TPS82671: Enable Control by 3851

Queation regaridng the TPS82671 Enable signal. I would like to use an RC delay circuit on the enable line.

WIll this work? If so, is there a maximum resistance value for the resistor?  


A: Re: TPS82671: Enable Control by 1129650

The most effective way to control the enable is to use a supervisor like the TLV803.

A RC circuit can be used as long as there are about 10uA available at VIH on the enable pin.

The enable pin will be in the M-Ohm range.