TPS61240 - does EN pin have an internal pull-down or pull-up resistor?

Q: Does TPS61240 EN pin have an internal pull-down or pull-up resistor? by 1818757

Does TPS61240 EN pin have an internal pull-down or pull-up resistor? EN pin can be floating?  Leaving this pin unconnected enables or disable the device?


Q: Re: Does TPS61240 EN pin have an internal pull-down or pull-up resistor? by 10449

The TPS61240 EN pin (enable pin) does not have an internal pullup or pull down resistor.  The pin must be actively pulled high or low to ensure proper operation. If the EN pin is left floating and is not actively plulled high or low, the logic state is undefined.